This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549最大V-



各位老师,我使用两片OPA549T驱动同一负载   一个使用-5V~55V供电  提供正向驱动   另一个采用-55V~5V供电  提供反向驱动  现在的问题是采用负电压供电的片子 工作异常  芯片报警内部温度高  输出信号幅值只能到-30V 而且 还有很大的直流偏压,请赐教,不胜感激。