使用OPA541搭建的并联电路,参考datasheet上的figure15,我的实际电路时换成了正相输入,主运放增益为5倍。我使用±30V供电,负载为7.5R时,当输入信号(DC)在-4.92 - -4.98V之间,波形出现震荡(f=6.4MHz,Vpp= 130mV)。但是将供电改成±35V时,输入在-4.92 - -4.98V之间不会震荡,而在-5.9 - -6V之间发生震荡。所以运放稳定性是不是和运放电源轨也有关系?如果有,这种关系能不能补偿呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用OPA541搭建的并联电路,参考datasheet上的figure15,我的实际电路时换成了正相输入,主运放增益为5倍。我使用±30V供电,负载为7.5R时,当输入信号(DC)在-4.92 - -4.98V之间,波形出现震荡(f=6.4MHz,Vpp= 130mV)。但是将供电改成±35V时,输入在-4.92 - -4.98V之间不会震荡,而在-5.9 - -6V之间发生震荡。所以运放稳定性是不是和运放电源轨也有关系?如果有,这种关系能不能补偿呢?
输出有接什么负载吗?多大的负载?
因为随着输入信号幅值的改变,输出振动有影响,是不是因为输入幅值的提高,输出电流也随之提高,加上探头测试相当于容性负载的影响,导致整个电路的品质因子Q改变,发生震荡。
方便的话, 您在输出端串联一个小的电阻试试呢?