This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
請教各位工程師
我想要設計一個Voltage/Current sensing circuit,我找到TIPD135這個文件,但是我的電流範圍是1uA~100mA,電壓範圍有1.2V~6.6V及-1.2V~-6.6V兩種。請問是否可以使用PGA281這個Programmable OP來達成呢?或是TI有其他相關產品可以達到呢?1uA這麼低的電流讓我很頭痛...感謝
您好
請問PGA281的Datasheet寫input range是VSN+2.5V~VSP-2.5V,表示可以正負電壓輸入,這樣用在負電壓量測,還需要OP來調整偏置嗎?謝謝