Other Parts Discussed in Thread: OPA350, TLC2272, TMS320C6678, DXP
第一步:找到对应芯片的CAD文件,以OPA350为例:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA350, TLC2272, TMS320C6678, DXP
第一步:找到对应芯片的CAD文件,以OPA350为例:
我也是同样的问题,入选
我怎样使用该元件呢?在Ultra Lib中没发现呀。画原理图需要TLC2272
生成封装后,原理图和PCB都是默认在后台打开的,这时要把PCB关掉重开,原理图直接双击就OK拉。
我在转换过程中出现问题如下,然后转换不成功,求解答,谢谢!
Symbol "TMS320C6678_CYP_841_A" renamed to "TMS320C6678_CYP_"
Symbol "TMS320C6678_CYP_841_B" renamed to "TMS320C6678_CY00"
Symbol "TMS320C6678_CYP_841_C" renamed to "TMS320C6678_CY01"
Symbol "TMS320C6678_CYP_841_D" renamed to "TMS320C6678_CY02"
Symbol "TMS320C6678_CYP_841_E" renamed to "TMS320C6678_CY03"
Symbol "TMS320C6678_CYP_841_F" renamed to "TMS320C6678_CY04"
Symbol "TMS320C6678_CYP_841_G" renamed to "TMS320C6678_CY05"
Symbol "TMS320C6678_CYP_841_H" renamed to "TMS320C6678_CY06"
Symbol "TMS320C6678_CYP_841_I" renamed to "TMS320C6678_CY07"
Component "TMS320C6678_CYP_841" renamed to "TMS320C6678_CYP_"
Ultra Librarian Lite 5.3.409 Process Report
TextStyle count: 25
Padstack count: 1
Pattern count: 1
Symbol count: 9
Component count: 1
Export
Warning: Symbol "TMS320C6678_CYP_" attribute "DESCRIPTION" references missing text style ""
@
I had the same problelm when i tried to convert the RM48L952ZWT.
And I just find out that being a Ultra Librarian version issue.
when I use v5.3.409 I met the "Unexpected symbol : ." error, just now, after i updated to the latest version of v5.3.478, the conversion finished smoothly...
So I compared the two YYYY-MM-DD_hh-mm-ss.txt files, and we can see the differences are the negative numbers: the lateset version use "0-num" instead of "-num" for better compatibility, and we can notice that in the yellow-highlighted line the "-0.xx" was being presented by "-.xx" which I believe was the cause of this error "Unexpected symbol : ."