This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教各位先进有关LM675非反向功率放大的问题
我要做的东西是利用将DAC(0V~5V)后的弦波三角波及方波透过LM675进行功率放大
LM675是依照这个电路
但输出波形(蓝色)却是这样(黄色为输入讯号)如下,不知为何会出现方波,我电路放大增益为2(R1、R2都用1k,其余参数皆照上图去接的)
电源部分现在是用电源供应器送14.5V,但输出电流却只有0.01A(电源供应器上显示)
想请问各位先进有没有什么想法能提供想法或建议非常感谢 !
了解,非常感谢 !
那这样我有另一个问题,为什么低于4V的话输出电压会冲到电源峰值,而不是输出0V或是其他较低的电压呢 ?
好哦,那請問一下OPA548的共模输入电压有到0v吗 ? 會不會像LM675一樣因為輸入電壓小於4V使輸出波形達到飽和 ? 顺便问一下共模输入电压的部分在datasheet的哪里呀 ?谢谢回覆
您好,
OPA548的共模输入电压有到0V,但达不到正的电源轨,到(V+)-3。
在数据手册第6页: