This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

将频率为30MHz,振幅为0.2V的正弦波信号放大到功率6~8W的TI的放大器(需求量大)选型问题?

Other Parts Discussed in Thread: TPS61178, THS6214

大家好!请各位大家帮忙解答以下问题,非常感谢!

我们公司的一个产品要求产生一个频率为30MHz和功率为6~8W的正弦波信号去驱动一个感性负载,

其感性负载的测试数据如下:

具体要求如下:

1)现有的微弱的正弦波信号:我们现在已经能产生30MHz精确的正弦波,但空载和频率为30MHz时的正弦波的振幅只有200mV,目前要解决将微弱的30MHz,200mV(0.2V)的正弦波信号放大到6~8W:

2)高频功率运算放大器:将以上的30MHz的正弦波信号进行放大,波形尽量不失真,TI的哪个型号能满足要求而且成本低些?       如果以上的高频功率运算不好选择,能否将30Mhz ,0.2V的正弦波信号先通过ADC驱动器芯片将电流信号转换为电压信号,然后再通过一个运放放大电压到30~36V,最后通过一个电流放大器(运放)放大电流到200mA,后面的两个运放用一个升压芯片将锂电池电压升高并供电,这样就整个放大电路部分用了3个芯片,感觉复杂了些?有没有用TI的2个芯片能解决的?或者3个TI的芯片哪些性价比高点?

3)升压电路:因供电采用聚合物锂电池,电压范围为3.3-4.2V,需要TI的升压芯片给高频运放供电,最终输出6-8W的功率;可参考输出有效电压30V-36V,输出电流200mA,可以是这个电压和电流,也可以其它的电压和电流,只要最终输出的功率为6-8W即可。

4)在满足以上要求的前提下,这此是用于消费电子产品需求量大,芯片封装尽量容易散热,总成本尽量低些;

请教TI 专家和高手们有什么好的电路或者元件选型?万分感谢!