This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于单电源仪表运放输入正负信号的问题



我想请问一下,如果我用3.3V单电源仪表运放来放大一个  - 414.12mV ~ + 414.12mV 的直流电压信号

仪表运放的Vref可以设置为1.65V 吗? 

如果这样的话,仪表运放输出的信号会在 1.65V 上下变化吗? 还是说1.65V以下的部分会被砍掉?

传感器输入的正负电压信号,需要和仪表运放共地吗?共地的话负电压会被抬升1.65V吗?如果不共地,仪表运放也可以正常工作输出差分信号吗