This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM311做过零比较器的电压电流与额定值差距过大

Other Parts Discussed in Thread: LM311

尝试用LM311搭过零比较器,1、3脚接地,4脚接VEE,7脚经5.1K上拉电阻接VCC,8脚接VCC,2脚输入峰峰值10mV、频率1KHz的正弦波。

用电压源/电流源提供VCC和VEE,设定VCC+15V,ICC15mA,VEE-15V,IEE10mA。但是实际供电时,ICC=15mA, VCC=1.83V,IEE=0,VEE=-15V;用示波器和电压表测量输出端(7脚)的电压,接近-15V并且没有变化

想不明白为什么VCC和ICC会这样,希望能有人解答一下

1. 这种情况芯片是不是坏了?怎么判断芯片的好坏?

2. 为什么会出现ICC远大于额定最大值而VCC小于额定值的情况?我该怎么操作才能实现过零比较功能?