Other Parts Discussed in Thread: OPA2140, OPA2364, OPA364, OPA140, OPA657, OPA656
您好!
我目前使用OPA2140作为对光信号做I/V转换的前置放大器,信号频率为50KHZ,光电流信号从2脚负端输入,光电流大小为PA级,反馈电阻为1M欧姆,反馈电阻并联1PF电容去燥,3脚输入2.5V的偏置电压,OPA2140供电为5V单电源,可是1脚输出值却一直是5V,我想了很久找不出原因,能帮忙分析下吗?非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
先回答第二个问题:此外,OPA2140能用于加减法放大吗?第二个运放是用于减掉2.5V偏压的,可实际实验结果却没减掉,而OPA2364可以。
OPA364是RRIO的运算放大器,即输入输出轨到轨。由于内部使用了charge pump,使得运放能够接受超过电源轨的信号。
Common-Mode Voltage Range VCM 负轨为(V−) − 0.1 正轨为(V+) + 0.1 V。
OPA140是RRO的运算放大器,即输出轨到轨放大器。输入并不是轨到轨。输入范围为:
Common-Mode Voltage Range VCM 负轨为 (V–) –0.1 正轨为 (V+)–3.5 V
因此如果使用5V供电,OPA140的有效输入范围为 -0.1 至 1.5。这就是为什么楼主第二级使用OPA140不能正常工作的缘故。
对于第一个问题:
"在相同光强下,光强较强时,OPA2140和OPA2364均有信号,但光强较弱时,OPA2364有信号而OPA2140没信号,难道OPA2140的最低电流响应还不如OPA2364?"
有可能同样是输入信号范围的缘故导致的,楼主可以做个实验,提高OPA140的供电压至10V,再比较一下实验结果。