This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA551输出失真,同样电路用OPA2604不失真

Other Parts Discussed in Thread: OPA551, LMC6034

大家好,我用LMC6034做了一个60KHz,3V左右的正弦波,然后进OPA2604,放大5倍左右,单电源30V供电,输出±15V左右的正弦波。然后我琢磨着2604只有20mA的输出电流,想要用OPA551做功率放大,同样30V单电源供电,放大5倍,可是输出只有±2V的三角波,失真了,这是为什么呢?SR和带宽,都满足要求的吖,参数和2604差不多。我有点着急呀!

  • 建议把波形和电路参数发下。
  • 您好,

    OPA551的输入共模电压范围是(V–) + 2.5 ~ (V+) – 2.5,如果单电源30V供电,即为2.5V~27.5V。另外OPA551也不是轨至轨输出运放。

  • 图1是电路图,LMC2604,OPA551,OPA07,都用的这个电路图。图2是2604的输出,30V单电源供电,输入是3v不到的正弦波。图3是OPA551和OPA07的输出波形。

  • 您好,看了下您的电路图,首先您的意思是输出+-15Vpp的正弦波,那么需要的SR=2*PAI*Vpp*F=2*3.14*30*60K=11.3V/us,而OPA551的SR为15V/us,所以压摆率的余量不是很多,我用您的电路图尝试了下,降低信号频率会改善很多。
    另外,单电源30供电,您目前输入是0~3V正弦,同相给了 15V 电压偏置? 这样的话输出会饱和。
    我用TINA仿真了下,降低频率,然后给3V偏置,输出是没问题的。

  • 非常感谢您的回复,确实有限幅,不过在应用里可以接受。我还有2个疑问,麻烦您在帮我看看。1,我曾经将放大倍数改为1倍和2倍,那么输出就是3V或者6V,SR会有充分的余量,但是输出还是不行,怀疑是芯片某宝买到假的了....2,OPA2604已经成功放大,接负载2K电阻,串联用手持万用表直流档测量,理论应该有几mA的电流,输出电流为何只有几十微安?手册里I0可以达到10mA的。而且我用数字万用表交流档测,测不到电流。这是什么原因呢?