Other Parts Discussed in Thread: OPA551, LMC6034
大家好,我用LMC6034做了一个60KHz,3V左右的正弦波,然后进OPA2604,放大5倍左右,单电源30V供电,输出±15V左右的正弦波。然后我琢磨着2604只有20mA的输出电流,想要用OPA551做功率放大,同样30V单电源供电,放大5倍,可是输出只有±2V的三角波,失真了,这是为什么呢?SR和带宽,都满足要求的吖,参数和2604差不多。我有点着急呀!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢您的回复,确实有限幅,不过在应用里可以接受。我还有2个疑问,麻烦您在帮我看看。1,我曾经将放大倍数改为1倍和2倍,那么输出就是3V或者6V,SR会有充分的余量,但是输出还是不行,怀疑是芯片某宝买到假的了....2,OPA2604已经成功放大,接负载2K电阻,串联用手持万用表直流档测量,理论应该有几mA的电流,输出电流为何只有几十微安?手册里I0可以达到10mA的。而且我用数字万用表交流档测,测不到电流。这是什么原因呢?