This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放的输出电压正常,输出电流很小,为什么

Other Parts Discussed in Thread: LMC6032

大家好,我用LMC6032运放,文氏振荡,产生了一个3V的正弦波,然后此信号进入6032运放做的电压跟随电路,输出端在进OPA2604,进行放大。目前输出电压正常,已经成功放大。可是接负载2K电阻,理论应该有几mA的电流,输出电流为何只有几十微安?手册里I0可以达到10mA的。而且我用数字万用表交流档测,测不到电流。这是什么原因呢?

  • 您好,

    输出电流只有几十微安,您是怎么测量的呢?因为输出的是交流信号,用万用表测量是一般测量的有效值,是测不出来的。最好在别的地方验证一下万用表交流档能够正确测出交流电流。
    ‘目前输出电压正常,已经成功放大’ 是指接负载2K电阻的时候,输出电压正常吗
  • 感谢回复!接不接2K负载,都可以放大。测出几十uA是用直流档测试的,而且还是运放Uo---黑表笔---红表笔---2K电阻---GND。