Other Parts Discussed in Thread: PGA281, OPA855, OPA657, OPA847
采用PIN管前端的TIA放大,要求捕获单个光脉冲信号,信号脉宽10ns,电流从10uA到100mA范围。
如何测量。需要多级放大每一级都加ADC么?有没有其他方案?
如果有两路信号,两个PIN管同时接收单个光脉冲,信号大小相差小于5倍,信号脉宽10ns,电流从10uA到100mA范围。
有办法分辨两个信号的相对大小么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
带宽比较大的可用于光电流应用的精度运放,可以看下OPA657(1.6Ghz),OPA847(3.9GHz)。