问题描述:LME49724运放设计中采用正负15V供电,上电后测量电压发现负15V电压值直线下降,正15V也有下降,但下降十分缓慢,导致运放发热严重;
然后采用正负12V供电,上电 测量电压,正负12V均正常,且没有下降的情况
查看芯片手册电压范围是±2.5V to ±18V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题描述:LME49724运放设计中采用正负15V供电,上电后测量电压发现负15V电压值直线下降,正15V也有下降,但下降十分缓慢,导致运放发热严重;
然后采用正负12V供电,上电 测量电压,正负12V均正常,且没有下降的情况
查看芯片手册电压范围是±2.5V to ±18V
对于高速运放,由于本身静态电流就比较大,所以;高压发热是个普遍现象。因此;推荐供电电压不要超过13.5V。
简单演算下,以LME49724数据表中第13页图49为依据。+-15V静态电流为9.35mA,静态损耗为0.2805W。按数据表第三页数据;结到空气热阻为49.6C/W。得温升14C。这样;以环境25C计,IC为39C手感略烫。如果没有散热覆铜;温升最高会达到3倍;约67C。静态手感都会非常烫;以至无法长时间接触了。带载发热更甚。
对于12V;静态电流约9.15mA,折合损耗为0.22W,温升不到11C,温度低了很多。