Other Parts Discussed in Thread: OPA857, THS4541, THS4521
none
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
改变输入电流后,OPA857输出与输入是线性的:
您好,相对来说比较方便的设计是使用您两颗OPA857,分别输出两个单端信号OUT接到后端THS4541上,然后再对THS4541的增益进行设置。 这样设计相对现在将1.83V输出接到THS4521的输入端要方便。
比如OPA857的CTRL=1, 那么Gain=20K。 0~2uA的电流输出电压范围为1.79V~1.83V,再分别将这两个信号接到THS4541的IN+和IN-端,设置增益,得到差分输出。
THS4541的输出您需要多大的共模电压?我看您这里设置800mV,为什么要设置800mV的Vocm?