Other Parts Discussed in Thread: PGA308EVM, PGA308



最近在用308做开发,出现了一些问题,请求各位大神给与解答:
最近在用308做开发,出现了一些问题,请求各位大神给与解答:原理图如图所示,实际连接中,用USB DAQ板对我的板子进设置,将我板子的VCC,GND和1W分别与USB DAQ板的J3插口的17脚,J4插口的25脚以及J3插口的11脚连接,两个输入则用直流电源提供毫伏级电压,输出连示波器,可能我的引线比较长;之后用软件进行放大倍数等设置时(在Block Diagram中改参数),改变输入电压,但输出都是杂乱的噪声,我分析是1W通信出现问题,然后在Register in RAM面板中,点击Read from RAM,显示单线超时,请各位大神给分析一下,这是什么问题,308芯片是新的,在刚打开软件时,也会出现单线超时,但过会就好了,我用的是Win 10系统,但用我电脑对308EVM就能正确配置,麻烦给位大神给与解答,谢谢。