Other Parts Discussed in Thread: OPA2187
例如OPA2187,输出10V的时候突然被短路会怎样?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不对,ISC是输出短路电流,是一个极限参数,即便你小于这个值10%,如果长时间通电都有可能烧掉芯片(对输出电流较大的IC),小电流的一般不会
亲;输出多少电压短路,与状态基本没啥关系。对于这款IC;最大(最高供电电压)短路典型电流为30mA。
由于楼主说的输出是10V,所以;该IC供电电源可能单电源10~36V或+-10~+-18V。
短路功耗为0.3~0.54W或0.3~1.08W。
OPA2187有两种封装,分别对应热阻为:159C/W和100.1C/W
对应理论温升为:47.7~85.86C/30.2~54.4 47.7~171.7C/30~108.1C
该IC理论结温上限为150C,因此;Tj理论温升+环境温度只要不超过150C,就是安全的。
例如;环温-25C时;这粒IC典型状态始终是安全的。反之;如果环温达到125C,该IC典型状态是热失效。
其它以此类推。