This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2917无输出电压



大家好,我使用LM2917做一个F-V转换,输入在40Hz-250Hz之间,希望输出电压希望在0.4V-2.46V之间。参考Figure19 ,C1选用103pF,R1采用82K,C2105pF。

实际测试不管1脚输入频率如何变化LM2917无输出电压,2脚始终为5V、3脚始终为0V、4脚始终为0V、6脚7.5V、Vout1=0V。

麻烦帮分析一下我哪里用的不对?

下附原理图及PCB图: