Other Parts Discussed in Thread: OPA637, OPA2132, OPA627
如上图参数,OPA637用在IV转换的时候,反馈电阻大于560R的时候,输出的声音直接有破音的声音。调低至560R就没有了。但是后级的LPF时,现在在信号源静音的时候,输出有噪音,噪音的类型有点像类似低噪声。请问这个是需要调整哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
其他同样的电路,用其他OPA627和OPA2132,OPA2111都没问题。只是用627的时候有噪音。
这些运放的渠道是一样的,而且可以保证是原装正品。同样的电路用其他运放完全没有那种噪声。在LPF的反馈电阻改为3.2K纯属是因为OPA637的稳定增益必须≥5db,所以才修改的反馈电阻。但是电阻改为3.2K就有很大噪声,如果使用之前627的反馈电阻是620R,这样的增益大约是-0.8db。噪声小很多,但是还是有一些。而且LPF输出我用一个10K的可调电位器做音量控制,在前端信号静音的时候,我扭动电位器,低频的喇叭振膜会有大幅度的移动。音量增大过程中,喇叭振膜往内移动,音量减小过程,喇叭振膜往外移动。而且移动的幅度和调整电位器的速度有关系,扭动速度越快,振膜移动的幅度就越大,停止扭动的时候,振膜会回复正常位置。反馈电阻大的时候,振膜移动会更明显。别的运放就不会有这种现象。就是感觉很奇怪。