This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

全功率带宽和运放的增益带宽的区别?

搜了太多资料,都说全功率带宽由压摆率决定,增益带宽是小信号的带宽。但是我还是非常疑惑,对于小信号,比如一个Vpp=100mV的正弦波,把他带入公式:

FPBW=SR/(2*pi*Vp)。

我能把小信号的50mVpeak带入其中计算得到GBW吗?

还是说计算FPBW的Vp必须等于电源电压的范围(或者接近输出轨到轨范围)?

为什么在考虑小信号的时候就不用考虑压摆率呢?同样是100mV的正弦波,假如某运放带宽100MHz,在Av=+1时,输出电压的最大压摆率

SR=2*pi*f*Vp=6.28*100M*50mV=31.4V/us。即使是小信号他的压摆率也不低啊?为什么就不考虑呢?还是如果这个运放的参数若如此,这个31.4V/us注定比它手册声称的压摆率要低?

另外一个问题:带宽,压摆率都是输出对输入的动态响应,假如我的输入不变,输出负载的动态响应看什么参数?还是带宽,压摆率?他们是怎么建立关系的,反馈吗?

菜鸟问题多,先谢过!