This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6521的增益问题

Other Parts Discussed in Thread: LMH6521

您好

电路情况是这样的

输入信号为200mV,脉宽为200ns的pulse信号,猝发周期为10ms。

信号前端使用ADA4932运放进行单端转差分,参考电压为2.5V。

ADA4932输出差分信号接入电阻衰减网络,阻抗为200欧姆。

然后接入LMH6521.

信号在LMH6521输入时为200mV,在LMH6521的输出侧,无论怎么通过SPI发送指令,他的输出幅值均无法满足理论计算的增益。

在SPI发送增益为00000时,即增益为26dB,200mV的输入信号经过LMH6521后,仅仅只有1.1V

想请TI的工程师麻烦看一下是怎么回事

谢谢