Other Parts Discussed in Thread: OPA1632, THS4521, PCM4204
想用THS4521替换PCM4204开发板上的OPA1632。在4521的数据手册上有替换电路:
但是THS4521的输入电压为(Vs-)-0.7~(Vs+)+0.7即为-0.7V~5.7V,而OPA1632的输入电压为(-Vs)~(+Vs)即-15V~+15V。现在需要的输入电压为-2V~+2V,请问用THS4521替代OPA1632会有问题么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
首先输入电压为(Vs-)-0.7~(Vs+)+0.7只是THS4521的绝对工作范围, 只是说明一个不损坏器件的输入范围.
能够让电路正常工作的话, 其推荐输入的范围是(-Vs-0.2V)~(+Vs-1.3V).
如果你的输入是-2V~2V, 直接用指标书推荐的0~5V供电工作会有问题.
解决方案是可以采用双电源供电. 只是电源电压有点尴尬. 比如-2V及3.3V供电. (你可以自己组合, 只要总的压差小于等于5.5V, 且正端留1.3V, 负端最高可以为-1.8V).
谢谢!