This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用TL3016和opa335构成的一个电流保护电路无法工作

Other Parts Discussed in Thread: TL3016, TL331, OPA335

 这里是想利用比较器的输出,在电流过大时,使比较器反向输出端输出高电平,通过二极管构成一个正反馈电路,从而使比较器正向输出端一直为低电平。

现在出现的问题是:上电时,如果R11过大,电路会直接锁上,比较器正向输出端会一直输出低电平。

所以有两个疑问:1.R11的阻值为什么会影响电路工作的状态?

2.TL3016的输入端是什么结构?因为这里R11接入的本意是希望两个二极管都没有导通时可以将比较器输入负端下拉到地。

  • 您好,

    信号VF2的输出波形是怎样的,是期望输出吗?可以把仿真文件附上吗

    对于TL3016我们只有datasheet可供参考,但datasheet没有提供其内部结构图。我们可以参考tl331比较器的输入结构,对比较器输入有个大体了解:

  • 仿真.TSC

    你好,这里r11使用2K和3k时,比较器会输出不同的波形。在2k时,开关闭合瞬间比较器不会形成反馈,在3k时则相反。

  • 您是检测的R5上的电压吗,建议您将前级输出信号换成交流电压源,如果OPA335输出没问题,就把这一级用信号源替掉,明确输入VF2信号至后级电路,现在这个电路我都不清楚输入信号是什么,范围是多少,怎样变化的,仿真只能打开关闭开关两种输入状态。