请问这样设计是不是错误的?只有+5V的供电,输入的是正的脉冲信号。我想设计两个反向放大电路。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA354是轨至轨输入输出的一款运放,当然也不是绝对能到电源轨,它的输出距离电压轨的压差典型值为0.1V,比如5V供电,输出能达到4.9V。
第一级如果想输出-5V~0V的范,那么OPA354不能满足要求,因为它的供电电压范围为2.5V~5.5V,双电源供电为+-1.25V~+-2.75V。 所以需要选择一款宽电压供电范围的运放来替代第一级。