Other Parts Discussed in Thread: TPA3255, TPS3802
按照TI的参考设计做了块TPA3255的功放板。输出模式为2.0 双桥。问题过程如下:
1:刚开始调试时,板子以一上电就不停的复位。查询相关问题时,看到有人提示断开输出LC试试。果然断开1uF的输出对地电容就正常了。
2:断开输出LC的1uF对地电容后,板子上电正常,但是带不了负载,音量10%以上,又出现3255不断复位。查询TI的LC的相关计算资料,修改输出LC的对地1uF电容为 跨接在AB上。(参考设计是A、B、C、D各对地有1uF的电容,改为:去掉对地电容,在A-B间和C-D间上分别跨接1uF的电容)。这样音量能开到30%左右。再开大又会不停复位。
3:实验发现:C-D桥能输出60%的音量,再大就进入不断复位的情况;A-B桥只能到32%音量就进入不断复位。
4:在3255不断复位时测量 reset脚电平对应着3255的复位变低,但是不是电源监视的TPS3802给的信号,3802监视的4V电压一直没有降低。
5:在3255不断复位时测量FUALT脚和CLIP_OTW脚电平都是高,没有观察到跳变。
6:复位的整体表现为声音顿卡,调低音量就能自行恢复正常。
补充:比如说在35%的音量,如果没有大的低音时,没有进入不断复位的情况;若有大的低音时就会进入不断复位的情况。 OC-ADJ过流电阻用的24K的。
请问现在该从何方向查找问题?
另外,功放板在30%左右的音量播放一天都很正常。 PVDD为 25V 。输出电感10uH。外接音箱为4欧姆。