您好,
想请问在只有单端输入的情况下,THS4531如何输出差分信号。
我的输入电压为0-5V,想通过THS4531输出0-3V的差分信号给DSP28377D。我用TINA做了仿真,发现了一些问题。
我将输入的0-5V的电压通过电阻分压至0-3V,输入到THS4531,得到的结果如图所示。
但是我想得到的波形是下面这样的。
不知道我应该怎么修改电路,期待您的回答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问我将输入电压从0-5V降至0-3V,再输入进THS4531,这样的方法可行吗?
您好,
对您上次说的为THS4531提供+/-2.7V电源会出现削波现象,以及输入至THS4531的电压最大为3.9V,我对器件进行了更换。
我将THS4531更换为THS4501,并对电路进行了修改。已知最初的输入为0-5V,我想输出的是0-3V的差分信号给DSP28377D的ADCIN引脚,请问下面TINA文件里的方案会不会存在什么问题?
谢谢!
您好,非常感谢您的解答。
针对您的回答我对电路进行了一些更改。
1.更改后的第一片OPA2277是低通滤波器,第二片是将输出电压降为+/-1.5V。
2.我的应用中的最高频率为5kHz,OPA2277的带宽应该能满足需求。
3.我已经将C12等一些电容去除。
4.我现在比较疑惑的一点是目前的最高输出只能达到2.94V,最低输出为55mV左右,并不能达到准确的0-3V。
请问您有没有什么方法能够将输出增加至0-3V,如果方便的话请在电路中进行更改,谢谢!