This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903电路设计分析问题?

Other Parts Discussed in Thread: LM2903

请问关于下图的LM2903电路,是基于什么原理?不清楚道理何在,烦请帮忙分析解惑,谢谢!

  • 您好,

    LM2903是双路比较器,同向输入信号与反向输入信号进行比较,输出一个高或低电平。
    如果用来检测3.3V电压,反向输入端应该是一个固定的电压值。您的电路是参考的哪里的电路呢
  • 我这是看别人的电路设计,觉得没有道理,但是他的所有比较设计、不只是3.3、24V、37V输出比较都是这么做的,设计初衷是比较输出后实现3.3>37>24V上电顺序的控制,可是这种接法反向输入端加电容直接到地,直流电压直接就被阻断了,不提供参考电压的做法,没有办法理解!
  • “设计初衷是比较输出后实现3.3>37>24V上电顺序的控制”不太明白,这个功能是已经实现的功能,还是处于开发调试阶段,完整的电路可以分享出来吗