This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA454电源供电问题

Other Parts Discussed in Thread: OPA454

TI 工程师及各位大神:

我目前想设计一个使用OPA454做的电压放大,输入信号0~3V(如图所示),期望放大15倍,输出信号为0~45V。

我想 让OPA454的V+为+48V, V-为-12V,即V+和V-的绝对值不相等,请问这样做可以吗?

我想这样做的原因如下:

1)输入信号只有正信号,但如果采用单电源供电的话,输入信号不符合OPA454单电源工作时 Vin>2.5V的要求,即小于2.5V的信号部分不会被放大。

2)如果采用V-为-48V固然可以满足OPA454的供电需求,但是-48V不易得到,而-5V或-12V比较容易获得。

多谢各位指教~