This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP07C单电源供电范围

我看OP07C规格书双电源供电范围可以达到±3 V to ±18 V,那单电源供电的范围是多少?是不是6-36V呢?

  • 单就单电源范围;确实可以达到6~36V。但考虑到共模抑制范围,建议6~24V。

  • 您好,

    经确认,OP07C只要总电源电压(V+) — (V-)大于6V小于36V就可以。但是,由于输入共模电压范围和输出摆幅是与供电电源有关的,因此使用时请注意OP07C线性输入电压范围和输出电压范围。

    为了不误导其他用户,我把我上一个不合理的回复删掉了。