Other Parts Discussed in Thread: LM2904B-Q1
亲爱的TI工程师,
我在项目里面,需要一款运放来做放大。因为有数字校准系统,所以对运放的输入失调电压大小没有多高要求。但是,对于输入失调电压的温度可重复性要求很高。举个例子:25℃时,Vos为1.200mV,将运放加热至100℃,然后冷却至25摄氏度,要求Vos在1.190mV到1.210mV范围内,前后误差不超过10uV。
不知道TI的普通运放里系列能否满足要求,比如:Vos范围为±3mV,是指每次回到相同温度点时,只能保证在±3mV之内,还是可以精确的回到某个Vos点。
如果不能精确的回到某个Vos点,是不是意味着只能选择Vos在10uV以内的精密运放了?
还请TI的工程师帮我解开困惑,谢谢!