Other Parts Discussed in Thread: OPA855, LMH6629
在使用LMH6629和OPA855做TIA放大器时,从上册上对比两个芯片的参数,感觉OPA855的带宽要大,输入电容要小,OPA855应该比LMH6629性能更好才对,但是实际测试时,性能却差不多,LMH6629还略微要好一点,OPA855的噪声略大,同样跨阻增益时,带宽略窄一些,这是什么原因呢?两块测试板使用的同样的APD,结电容1pF,跨阻20K,Cf0.05pF。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我这边做的两个放大器输出波形都是稳定的,没有震荡,满足最小稳定增益。
下图分别是OPA855和LMH6629的噪声密度,可以看出OPA855电压噪声密度0.98nV/根号Hz,电流噪声密度2.5pA/根号Hz.LMH6629电压噪声密度0.69nV/根号Hz,电流噪声密度2.6pA/根号Hz。可以看出LMH6629的噪声特性确实要好一些。但是在看两者的输入电容,OPA855的输入电容是0.8pF,LMH6629的输入电容是5.7pF,显然LMH6629的结电容会大很多,这样讲就会导致噪声增益大很多,噪声密度小那么一点顶不住增益大好多倍,且在相同跨阻情况下,LMH6629能做到的最大带宽会窄。但是实际情况刚好是相反的,LMH6629的噪声和带宽都要比OPA855要好些。这个不知道是什么原因?