,之前没有接触过这类放大器,datasheet中给的参考电路负反馈回路都有电阻,但是这个原理图中没有,Uout1是一个恒定的可以设置的电压,re是一个电极,放大器输出连接的是一组功率三极管连接的推挽电路。自己测试,上电,RE不连接,RE=0V,Uout1=0.045V,输出是个11v+。re连接上3.3v,输出是个3.5v左右,毫无规律。这版电路是接手的前人的,但是最初是抄的别人的,至今弄不明白。想请教论坛里的大侠,(1)这个放大器有无图中这种连接方式,实现的功能是什么?(2)流程中测量RE的电压是变化的,单片机程序中,Uout1也是变化的,估计是在保持某种关系,这个电路如果正确,有没有确定的输入输出的关系式???如果还有什么想知道的,请问我,知无不言。