This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AMC1200输出共模电压1.29V问题

Other Parts Discussed in Thread: AMC1200

请教一下,关于AMC1200输出共模电压1.29V,如果我将VDD2输入是正负电压,这个1.29V可以变成0V吗?

  • 这或许是可行的,但由于未经过全面测试,因此不能保证以这种方式操作设备时的行为。对于您的操作货有些担忧,尤其是对于共模输出电压。如果查看器件数据手册,将会看到共模输出电压通常为1.29V,但最小值为1.15V,最大值为1.45V。如果以单端方式进行检测,则共模输出电压的任何变化都将导致直接失调误差。
    总而言之,建议使用单极性电源操作该器件,使用运算放大器进行电平转换和差分至单端转换。