Other Parts Discussed in Thread: INA240
INA240的输出需要进行一个低通滤波吗,INA240的Pin_8输出管脚的电压信号需要接一个低通滤波吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA240
INA240的输出需要进行一个低通滤波吗,INA240的Pin_8输出管脚的电压信号需要接一个低通滤波吗
你好,我今天在做ina240采集时,发现一个问题。我芯片ref1接地,ref2接参考电压+2.5v。当差分输入电压为0是,芯片输出管脚怎么是1.25v,正好是ref2电压的一半。据我所知,当差分输入电压是0v是,输出应该是2.5v啊。这是怎么回事。望速回,等待中。
噢噢,我知道了。输入的差分电压是正的话,芯片输出电压就会以1.25v做参考点往上增长。最大增长到vcc,如果输入差分电压是负的,就会以1.25v往下减,最大只能减到0v对吗。
您好,INA240的输出不是VCC/2,是不是和VCC的纹波有关系? 我发现VCC的PK-PK范围越小,无输入时候输出越接近VCC/2.
120mV纹波的时候,输出1.6V。30mV纹波的时候,输出1.88V。
INA240对VCC的纹波有要求吗?具体多少呢?
谢谢。