This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4304放大电路仿真问题 路过的各位指导下啊,

Other Parts Discussed in Thread: THS4304, THS4303

请教各位大佬,我做的关于THS4304的仿真结果总有问题,路过的各位指导下啊,这是什么原因啊,怎么改呢?用了TINA 和multisim仿真都是一样~~~~

正负2.5V电源供电可以实现放大功能。

5v供电时,在同相输入端加了2.5v的偏置,信号源用的是偏置5mv,振幅1mv的正弦电压信号,同样的放大电路配置,但是无法实现波形放大了,输出一个1v左右的电压信号,该信号里面叠加了一个很小nv级的正弦信号。

按照芯片手册上的电路仿真的也无法实现放大。。。