Other Parts Discussed in Thread: BUF602, LM358
这个电路原来是PWM控制输出0—10V,1mA的。如果输出10mA会有1V的压降
现在客户要求输出0-10V,10mA,不能有压降,如何提高运放的带载能力?我修改了下线路图,把运放的第二级接入作为缓冲,这样是否可以?感谢各位指导。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,1mA输出的时候我只用了LM358的一个通道,第二个通道没有用
我修改后的下面的线路图就是把LM358的第二个通道接进去作为buffer,这样可以吗?
明白,我是想看理论上这样是否可以。我测试了下修改后的线路,因为在运放输出端接了两个47R的电阻串联,所以负载10mA的时候会有接近1V的压降,把电阻去掉就是10V,10mA没有压降了,感谢您的指导!