Other Parts Discussed in Thread: PGA308, XTR116, PGA308EVM
请高手指点,我在做PGA308+XTR116时,Block Diagram可以检测到压力信号,如图

可是在calibration中怎么就检测不到信号呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Huang ping,
1,PGA308+XTR116可以有好几种配置模式:
建议您按照以下步骤测试:
下面是把PGA308配置为4-wire电压输出,旁路掉XTR116的测试方法,如果校准完成,调整传感器的输出,可以用万用表测出Vout_f的电压是在0.5~4.5V。
(注意,此时不需要给USB_DAQ板上的T1和T2供电,因为没有用到电流环输出电路,只是用PGA308对传感器校准,输出电压信号)
USB_DAQ板的硬件配置,详见:
PGA308 (配置为4wire)电压输出,把XTR116Bypass掉,PGA308EVM硬件配置详见:
用万用表检测 T3的VEXC、Vs、Vref输出是否正确。
对应的软件校准操作,详见下图,注意选择pre_vout_4p096.csv文件,然后按照提示调整传感器的输出电压,完成校准: