This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于工频干扰的疑问

各位老师好:

电路设计过程中,经常会考虑到工频干扰,用的最多的无非就是用陷波器处理。最近我在做心电图仪的时候,发现心电信号大致范围在0.05~100Hz。也就是说心电信号中含有50Hz,60Hz的信号,如果使用陷波器除去,岂不是会把有用信号也除掉?

该怎么处理有关工频干扰的问题?谢谢。

  • 1、从信号系统的角度,对于心电信号采用50hz notch filter是不正确的。因为心电信号本身包含了这个频段的成分。另外,非线性相位的陷波器同时还会引入相位失真。

    2、很多老的文章和应用中采用了工频陷波器,这主要受到技术限制的历史原因。就像物理学中的,电流方向被规定为“正电子运动方向“一样。包括设计者和医生都是适应了这种系统。有一些产品中甚至还使用了,低于50Hz的低通滤波器。

    3、一方面,工频干扰对于心电人体模型是共模信号。所以,对于工频干扰的抑制,应当通过提高系统的共模抑制比来实现。另一方面,随着数字系统的普及,复杂的运算得以轻易实现。现代已经有很多论文讨论高精度ECG的做法。从而得到更为真实的心电波形和实现尽可能小的失真。关于这方面的深入了解,楼主可以在IEEE里面搜索到不少文献。