This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI 导入spice模型失败,提示语法元素错误,有什么特别要求,不能使用的语法么?

Other Parts Discussed in Thread: TINA-TI

您好,在使用TINA-TI 导入器件的Spice模型时,提示错误语法元素错误,不能导入器件,其spice内容如下:烦请知道,非常感谢!

* DRB501VM-40 D model
* PKG: UMD2,Vr=40V,Io=100mA
* Model Generated by ROHM
* All Rights Reserved
* Commercial Use or
* Resale Restricted
* Date: 2016/04/08
.MODEL DRB501VM-40 D
+ IS=1.8328E-6
+ N=1.1427
+ RS=.89254
+ IKF=12.564
+ XTI=2
+ EG=.6100
+ CJO=23.035E-12
+ M=.42022
+ VJ=.3905
+ ISR=2.110E-6
+ NR=1.3000
+ BV=45.000
+ TT=0
+ TRS1=0.0070