This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,INA128,输入电压是0.2V,放大倍数1倍,在实际测试中,V+-V-=0.2V电压,用电源箱供,运放供电双电源±15V,理论上,INA128输出得0.2V,但是实际测试,电路板1号:放大1倍,其输出只有0.183V,不满足输出电压2%的技术指标,但是放大25倍的时候,输出电压4.98V,可以满足技术指标,放大50倍的时候,输出电压9.95V,可以满足技术指标;电路板2:放大1倍,其输出只有0.181V,不满足输出电压2%的技术指标,放大25倍的时候,输出电压4.86V,不满足技术指标,放大50倍的时候,输出电压9.86V,不满足技术指标,请教大神帮忙看看电路,有没有什么问题,为何导致输出电压与理论值相差这么大?其中考虑过增益误差、线性度等,但实测值不应该和理论值差这么多。
您好,两个电路板的输出都是在INA128的输出端Pin6 那里测试的吗?
INA128能够驱动容性负载的能力为1000pF。您这里接了一个大的负载电容, 如果输出串联电阻的话,R74建议用小阻值去隔离,比如22ohm或者100ohm以下电阻。
您好,2脚是V- ,不一定要接GND,只要保证它的电压范围在输入共模电压范围之内就好。
关于第一路接入电源放大50倍是8点多V, 第一路电源最大6V吗? 因为INA128 输出电压距离正压轨的压差最小为1.4V,典型为0.9V,也就是说,如果10V供电,输出电压典型值为9.1V,最小为10-1.4=8.6V,是达不到10V电压轨的。
所以要保证供电电压够才行。