This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1675前端电路

Other Parts Discussed in Thread: INA103, OPA627, THS4503, ADS1675

分别采用OPA627构建电压跟随器,INA103仪表放大器进行一级放大后,再加电压跟随器(原因是不加电压跟随器直接将INA103输出接THS4503后,整体表现为衰减),后端采用THS4503搭建二级放大电路。具体电路为下图所示。一级放大实现10倍或100倍放大,二级放大采用1倍、2倍、5倍、10倍放大。

我想请教的问题是:

1.为什么单独测试两级放大都是正常的,但两级放大级联之后就呈现衰减,需要在两级之间加上电压跟随器才能够实现正常级联放大?

2.当两级通过电压跟随级联之后,大部分放大倍数是正常的,但是为什么第一级放大100倍,二级放大2倍时整体电路呈现衰减的状态?

3.为解决问题2,我在电压跟随器反馈上加了一个100pF的电容就解决了这个问题,请问这是为什么?

4.新的问题是此电路只能单端(实际上是伪差分)的时候所有放大倍数是可以的,但差分输入(将负端接地电阻去掉)还是衰减,请问是为什么?

希望您解答疑惑,谢谢