This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OPA858放大器仿真

Other Parts Discussed in Thread: OPA858

大家好!

想咨询下OPA858跨阻10M欧,正端接地,+-2VDC电源,负端输入正弦波峰值200pA电流,仿真可以达到线性放大2MHZ左右,为什么实际电路只有5KHZ以下是线性放大的?

  • 您好,跨阻运放在-3dB下的稳定带宽公式如下,可以看到,运放的GBP是一定的,稳定带宽是和Rf,总的寄生电容Cs成反比的,Cs等于芯片的输入差模电容Cdiff,共模电容Ccm,以及光电二极管的寄生电容Cd的总和。所以我们可以根据这个公式计算下稳定在-3dB的带宽是多少。

    另外,实际测试的波形可以附上看下吗?

  • 谢谢回复!
    按仿真1MHZ频率应该是线性放大-40dB,峰峰值应为1mV,而实际放大了峰峰值为50mV左右,相差50倍,再说1MHZ频率寄生电容影响有限吧?会不会我们手头采购的芯片有问题?仿真效果与实测
  • 最近我也在使用OPA858。我有点好奇,你手上有1G的电阻啊

x 出现错误。请重试或与管理员联系。