ADC12D1000的输入为-400mV到400mV,对于正弦波输入没有问题,但是想对一个脉冲信号采集,例如0-800mV的正脉冲信号,通过LMH6554后,如何让其工作在-400mV的偏置电压下,否则,ADC只能接收0-400mV的信号,-400mV到0的部分就浪费了。如何用LMH6554差分放大器将一个只有正脉冲的信号,转成-400mV偏置下的脉冲信号,即当输入单端信号为0时,ADC端采集到-400mV?当输入单端信号为800mV时,ADC端采集为400mV?多谢了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC12D1000的输入为-400mV到400mV,对于正弦波输入没有问题,但是想对一个脉冲信号采集,例如0-800mV的正脉冲信号,通过LMH6554后,如何让其工作在-400mV的偏置电压下,否则,ADC只能接收0-400mV的信号,-400mV到0的部分就浪费了。如何用LMH6554差分放大器将一个只有正脉冲的信号,转成-400mV偏置下的脉冲信号,即当输入单端信号为0时,ADC端采集到-400mV?当输入单端信号为800mV时,ADC端采集为400mV?多谢了。