This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA615IDR在输入为0V时,输出有200mV左右的直流电平

Other Parts Discussed in Thread: OPA615

       我们在OPA615IDR应用过程中发现个问题,OPA615IDR原理图如下图,在OPA615_IN网络悬空时,上±5V电压后,在ADC网络上有些OPA615芯片
能测到200MV左右直流电平,导致这种芯片只能检测输入端>200MV的峰值电压,如下表颜色黄色列是有问题的芯片,且问题现象跟着芯片走。
       按理说,当OPA615的10脚输入为0V时,2脚输出0V才是正常的,希望有高人帮忙分析一下,谢谢!