OPA140的datasheet中关于输入共模电压范围如下图,低于正电源轨3.5V,可是后面的图表中,电压跟随器电路,输入18.5V峰值正弦信号竟然跟随到电源电压18V!!我理解共模电压同相、反相端相等,始终等于输入信号,也就是共模电压也是18.5V峰值正弦信号,当这个正弦信号幅值超过18-3.5时,运放输入端就应该饱和,运放输出锁定到某一个电源轨,理解有问题吗?
话说,可以给OPA140正负5V供电,同相端输入峰值3.3.V/110KHz的正弦信号,输出能很好的跟随吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA140的datasheet中关于输入共模电压范围如下图,低于正电源轨3.5V,可是后面的图表中,电压跟随器电路,输入18.5V峰值正弦信号竟然跟随到电源电压18V!!我理解共模电压同相、反相端相等,始终等于输入信号,也就是共模电压也是18.5V峰值正弦信号,当这个正弦信号幅值超过18-3.5时,运放输入端就应该饱和,运放输出锁定到某一个电源轨,理解有问题吗?
话说,可以给OPA140正负5V供电,同相端输入峰值3.3.V/110KHz的正弦信号,输出能很好的跟随吗?
您好, 共模电压的理解没问题, 但是按照OPA140的输入共模电压范围,+-18V供电,输入正压不能超过14.5V. 所以+-18.5V输入是不允许的.
这里的电压跟随,输入超过共模电压范围,输出饱和,最大正向饱和电压为(V+)-0.2V. 可以看到有0.2V的削波.
所以实际应用中,+-5V供电,不建议3.3V输入, 要满足输入(V+)-3.5V的共模范围,所以3.3V输入.供电电压最小为6.8V, 因此提高供电电压, 使其正常工作.