This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4521输出电压跳动问题

Other Parts Discussed in Thread: ADS1220, THS4521

电路图如下图所示,THS4521电流放大10倍,差分输出用ADS1220再放大64倍后AD采样值跳动非常厉害,ADS1220不放大则跳动不厉害,用别的运放电路则不存在这个问题。是什么原因呢?

  • 您好,
    感谢您对TI产品的关注!
    电路中IS2+和IS2-是差分信号吗,您是要放大电流信号吗?我不太明白您的输入信号是怎么连接过来的,您可以给出信号源到THS4521输入端的完整电路吗,因为您说“THS4521电流放大10倍”我没看到增益电阻
    或者说THS4521能按期望输出吗?
  • 就是电流采样电阻两端各串一个1K电阻就到IS2+和IS2-,是差分信号。我需要检测电流0.1~100A的电流,误差在千分之五之内。
  • 电流采样电阻两端各串联1K电阻到IS2+和IS2-,那么THS4521这一级的增益是100,因为反馈电阻是100K。
    您有测THS4521输入和输出信号吗,是按期望输出的吗,建议您断开后级ADS1220电路,排除后级电路影响,先验证THS4521能够正常工作
  • IS2+和IS2-分别串1K电阻后短路,如果不焊C90、C98,VOUT+和VOUT-两端没有电压;如果焊上C90、C98,VOUT+和VOUT-两端则有十多mV电压,为什么?
  • 您是将输入短路吗,是我下面TINA仿真的那样吗?我TINA仿真的现象是接不接C90、C98输出都一样:

    您可以再检查下焊接情况,或者多测几块板子,排除焊接造成的问题

    4521.TSC

  • 我没有仿真,我是实测,应该不是焊接的问题,我试几次了。有更直接接的问题解决方式吗,这样一问一答太没效率了,我的电话:13535583355
  • THS4521在输入为0时,输出差分电压达不到电源轨,即达不到0V,在数据手册电气表格中可以看到在VS+ = 5 V, VS– = 0 V, VOCM = open时输出电压低电平典型值为0.10V,我用TINA仿真的为13.87mV,接不接C90、C98输出都一样的,是符合数据手册中电气性能的。
    因为输入的是0V,没有交流信号,因此理论上接不接C90、C98输出应该也是一样的。如果测试多块电路板还存在这种情况,那么您可以给出测试时详细的电路图接法图吗