This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题。返回报错。
ERROR - OTP Progamming was NOT successful. Please check the 'Error' Tab for more information
ERROR - Register 026A, was programmed to: 22, but read back: 00
ERROR - Register 0269, was programmed to: EF, but read back: 00
ERROR - Register 0268, was programmed to: 80, but read back: 00
ERROR - Register 0267, was programmed to: A3, but read back: 00
ERROR - Register 0266, was programmed to: 0D, but read back: 00
ERROR - Register 0265, was programmed to: F5, but read back: 00
ERROR - Register 0264, was programmed to: 0D, but read back: 00
ERROR - Register 0263, was programmed to: 25, but read back: 00
ERROR - Register 0262, was programmed to: 93, but read back: 00
ERROR - Register 0261, was programmed to: E4, but read back: 00
ERROR - Register 0260, was programmed to: 09, but read back: 00
ERROR - Register 025F, was programmed to: 50, but read back: 00
ERROR - Register 025E, was programmed to: 20, but read back: 00
ERROR - Register 025D, was programmed to: 94, but read back: 00
ERROR - Register 025C, was programmed to: EE, but read back: 00
ERROR - Register 025B, was programmed to: C3, but read back: 00
ERROR - Register 025A, was programmed to: 83, but read back: 00
ERROR - Register 0259, was programmed to: AE, but read back: 00
ERROR - Register 0258, was programmed to: 0D, but read back: 00
ERROR - Register 0257, was programmed to: F5, but read back: 00
反回全0说明芯片读写都失败了,可能芯片没有工作或连接有问题.需要确认是否正常上电,连接是否正确?