Other Parts Discussed in Thread: INA156, OPA2350
这是一个热电偶的信号调理电路,问题:当模拟开关选择一倍放大电阻时偏执略小于1V(等于我的偏执电压Vmid),随着放大倍数的增加(反馈电阻增大)到八倍时(6.8K)输出偏置电压几乎降到0。专家认为是什么原因那?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
然后将INA156的输出拉一个1K电阻到Vmid(加输出偏置),但是这样做了以后发现怎么加不上去,电阻一边是1V,一边是0V。
一个理想源和一个1K的输出阻抗的源加权平均,得到的肯定是一个理想源的值。
本意是在INA156 的REF加入Vmid,但是发现短接输入时偏置输出电压比Vmid小了100mv(900mv),所以对后面的差模放大来说反向端大了100mv,再经过放大所以偏执电压降到下轨。
楼主用的测试信号是什么频率的?测试信号是信号源还是传感器?测试信号和电路的连接是怎么样的?
P.S. 强烈建议楼主学会使用TINA进行电路仿真。方便讨论,提高效率。毕竟文字表述不直观也不方便讨论。谢谢!