Other Parts Discussed in Thread: SN74AHC125
SN74AHC125PWR缓冲器使能脚OE为高时,应该是没有输出的,但实际有大约1mS的输出,黄色1通道为1Y输出,蓝色3通道为1A的输入.在使用SN74AHCT244PWR缓冲器就没有问题,请帮忙解答,谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74AHC125
SN74AHC125PWR缓冲器使能脚OE为高时,应该是没有输出的,但实际有大约1mS的输出,黄色1通道为1Y输出,蓝色3通道为1A的输入.在使用SN74AHCT244PWR缓冲器就没有问题,请帮忙解答,谢谢!

您好,
感谢您对TI产品的关注!
SN74AHC125PWR的输入信号CONTROL-FAN-IN和XRS_BUF看示波器截图应该都是3.3V电压,而供电是5V供电。SN74AHC125PWR在5V供电时,SN74AHC125PWR可以正确识别的最低的输入高电平电压为3.5V(0.7*VCC),最高的低电平电压为1.5V(0.3*VCC),在1.5V~3.5V之间电压不能准确识别高低电平。因此,SN74AHC125输入3.3V的电压不能准确识别。
对于SN74AHCT244PWR,其输入高低电平范围不受供电电压影响,VIH(min)为2V;VIL(max)为0.8V,因此,输入3.3V的信号,可以正确识别高低电平。