This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA-400Q1-EVM下载程序返回读0或读0XFF,求解决,多谢。

硬件连接如图,四个LED均亮。上位机软件未进行任何设置,初始状态下进行HEX文件选取和下载,总会出现如下错误:

ERROR - OTP Progamming was NOT successful. Please check the 'Error' Tab for more information
ERROR - Register 026A, was programmed to: 22, but read back: 00
ERROR - Register 0269, was programmed to: EF, but read back: 00
ERROR - Register 0268, was programmed to: 80, but read back: 00
ERROR - Register 0267, was programmed to: A3, but read back: 00
ERROR - Register 0266, was programmed to: 0D, but read back: 00
ERROR - Register 0265, was programmed to: F5, but read back: 00
ERROR - Register 0264, was programmed to: 0D, but read back: 00
ERROR - Register 0263, was programmed to: 25, but read back: 00
ERROR - Register 0262, was programmed to: 93, but read back: 00

......

有时候读返回是0XFF,不知怎么回事,求各位大哥哥大姐姐知道。感谢。灰常感谢。期待很棒的你们的回答。